Using a Custom Application or Standard Application with a Sideloop - Metasys - LIT-12011829 - Field Device - VMA18 VAV Modular Assembly

N2 VMA Application Note

Product
Variable Air Volume > Modular Assemblies > VMA18 VAV Modular Assembly
Document number
LIT-12011829
Revision date
2018-11-01

If you created or edited the application using CCT, use the PRN file generated from the Advanced tab - N2 Mapping. This PRN file is in the same directory as the saved CAF file.