Troubleshooting - Metasys - LIT-1201535 - Supervisory Device - Network Engine

N1 Migration with the NIE Technical Bulletin

Brand
Metasys
Product name
Network Engine
Document type
Technical Bulletin
Document number
LIT-1201535
Revision date
2019-04-09
Language
English

Be sure to configure the Network Name attribute of the N1 Migration. Once you insert the N1 Migration, you cannot edit the Network Name attribute. The workaround is to delete the existing N1 Migration and insert a new N1 Migration ensuring you enter the desired Network Name before completing the Insert Integration Wizard.

Note: Be aware that the Auto Discovery process degrades the performance of applications running at the NCM (such as Trend), as well as any client applications (such as an OWS), which are collecting data.