System Configuration Tool (SCT) - Metasys - LIT-1201535 - Supervisory Device - N1 Network Engine

N1 Migration with the NIE Technical Bulletin

Product
Document number
LIT-1201535
Revision date
2019-04-09

The SCT assists in all phases of engineering, installing, and commissioning of the Metasys system devices. The SCT, an offline tool, creates NIE and NAE archive databases that can be downloaded to the Metasys system devices. The SCT uses the same UI as the NAE/NIE and the ADS or ADX. Use the SCT offline to define the Site Director.

Note: An ADS or ADX is automatically added as a Site Director. When you add more than one ADS, the second is added as a child of the Site Director. Only one Site Director can exist on a site.

You can upload device databases modified in the Metasys system to the SCT for archiving or editing. The SCT includes features to enable the synchronization of the archived and online databases.