Network Integration Engine (NIE) - Metasys - LIT-1201535 - Supervisory Device - N1 Network Engine

N1 Migration with the NIE Technical Bulletin

Product
Document number
LIT-1201535
Revision date
2019-04-09

The NIE is a web-enabled supervisory controller for integration of N1 Networks into the Metasys system. The NIE supports the same object set as the NAE; however, the NIE does not support field busses, specifically no N2 bus support, no BACnet® Master-Slave/Token-Passing (MS/TP) bus support, and no LonWorks® network integration. As shown in the following example, the NIE UI is similar to the NAE UI.

Figure 1. NIE User Interface in Focus View