Network Automation Engine (NAE) - Metasys - LIT-1201535 - Supervisory Device - N1 Network Engine

N1 Migration with the NIE Technical Bulletin

Product
Document number
LIT-1201535
Revision date
2019-04-09

The NAE, an Ethernet-based supervisory controller, provides features including alarm and event management, trending, archiving, energy management, data exchange, scheduling, dial features, and password protection through the web browser user interface.