NCM Object - Metasys - LIT-1201535 - Supervisory Device - N1 Network Engine

N1 Migration with the NIE Technical Bulletin

Product
Document number
LIT-1201535
Revision date
2019-04-09

The NCM object (Figure 1) represents one NCM in the Metasys system. All mapped objects within the NCM are under the NCM object. The NCM objects in the NIE are grouped underneath the N1 Migration object.

Figure 1. NCM Object