Launcher - Metasys - LIT-1201535 - Supervisory Device - Network Engine

N1 Migration with the NIE Technical Bulletin

Brand
Metasys
Product name
Network Engine
Document type
Technical Bulletin
Document number
LIT-1201535
Revision date
2019-04-09
Language
English

The Launcher is a software application that lets you use the SMP or SCT UI to access the Metasys system, server, or supervisory engine on the building network, regardless of its software version. To launch the SMP or SCT UI, download and install Launcher. For more information regarding the Launcher, refer to Launcher Installation Instructions (LIT-12011783) or Launcher Tool Help (LIT-12011742).

Contact your local Johnson ControlsĀ® representative for access to the Launcher software.