File Parsing - Metasys - LIT-1201535 - Supervisory Device - Network Engine

N1 Migration with the NIE Technical Bulletin

Brand
Metasys
Product name
Network Engine
Document type
Technical Bulletin
Document number
LIT-1201535
Revision date
2019-04-09
Language
English

The N1 Migration Tool parses global files and Network Controller (NC) DDL files from the N1 Network to import them into the Metasys system. File parsing breaks a file down into parts that a program can understand. In this case, the tool breaks down the global and NC DDL files into parts that the SCT can analyze and understand in terms of the Metasys system.