Table 1 lists the NIE factory-default configuration.
|
Field |
Value |
|---|---|
|
NIE55 Device Name |
NIExxxxxxxxxxxx, where xxxxxxxxxxxx is the Ethernet MAC address of the device in hexadecimal. For example, if the Ethernet MAC address is 00-80-66-05-0f-fc, the device name is NIE008066050FFC. |
|
DHCP Client |
Enabled by default. However, Dynamic Host Configuration Protocol (DHCP) must be disabled for communicating to the N1 Network. N1 Networks do not support DHCP. |
|
NIE55 Serial Port One |
115,200 baud, 8 bits, no parity, 1 stop bit (115200,8,n,1), Direct Connect IP over Point-to-Point Protocol (PPP). |
|
NIE55 Serial Port Two |
8 bits, no parity, 1 stop bit (9600,8,n,1) |
|
Site Director |
The NIE is a Site Director by default. That is, it contains a Site Object. If it should not be a site director, it must be demoted and the host name or IP address of the Site Director specified. |
|
Default NIE UI Login |
MetasysSysAgent |
|
Default NIE UI password. The NIE password is case sensitive. |
[default password] |