Network Map - Metasys - LIT-1201535 - Supervisory Device - Network Engine

N1 Migration with the NIE Technical Bulletin

Brand
Metasys
Product name
Network Engine
Document type
Technical Bulletin
Document number
LIT-1201535
Revision date
2019-04-09
Language
English

A Metasys N1 Network consists of at least one NCM, all the devices connected to this NCM, and all the hardware and software objects associated with these devices. The Network Map (Figure 1) displays the organization of the most recently activated network. The Network Map:

  • displays the network, PC group, system, device, and PC file

  • provides quick access to summary information within facilities

Figure 1. N1 Network Map