After Migration - Metasys - LIT-1201535 - Supervisory Device - N1 Network Engine

N1 Migration with the NIE Technical Bulletin

Product
Document type
Technical Bulletin
Document number
LIT-1201535
Revision date
2019-04-09

After performing an N1 Migration, use the NIE UI (accessed through a web browser) as the primary interface for your Metasys N1 Network (rather than OWS).

Keep in mind that after migration, conventions of the Metasys system apply to objects in the NIE UI and the SCT. For example, the Metasys system uses BACnet compliant units, as opposed to earlier versions of Metasys software where units were text fields. During an N1 Migration, the system attempts to establish Units type matches where possible. Units not matched are included at the end of the Description field for the object.