Mapped Names - Metasys - LIT-1201535 - Supervisory Device - N1 Network Engine

N1 Migration with the NIE Technical Bulletin

Product
Document number
LIT-1201535
Revision date
2019-04-09

The mapped names are the names objects have in the Metasys N1 Network. The N1 integration software uses this value to locate and communicate with the Metasys N1 Network object. The Migration server rebinds to this name every time it restarts. If the name changes in the N1 Network, the Metasys system object goes offline. The mapped names are in the form systemname.objectname.