Import Wizard - Metasys - LIT-1201535 - Supervisory Device - N1 Network Engine

N1 Migration with the NIE Technical Bulletin

Product
Document number
LIT-1201535
Revision date
2019-04-09

The Import Wizard guides you through the process to import a point definition file from a LonWorks network or a Metasys N1 Network. The Import Wizard creates points using the files created by the N1 Migration Tool and stores them in either an archive database (if you are offline in the SCT) or directly in an NIE’s database (if you are online with an NIE). You can only import the user view online to an NIE or ADS/ADX that is a Site Director; however, you can import the point definition files generated by the N1 Migration Tool to any NIE.