Online generation occurs at the NIE and operates against all the devices defined on the site. Add the N1 Migration, NCM, and mapped point objects under one or more NIEs. See Generating an NIE Database Online Using Wizards. The process is similar to the N2, BACnet®, and LonWorks integrations. Online generation uses the existing Metasys system Object Creation Wizards (Insert-Integration, Insert-Field Device, and Insert-Field Point) to create the database. You can also import the files that are generated by the N1 Migration Tool by right-clicking the N1 Migration object and selecting Import Integration from the menu that appears.