Offline database generation occurs at the SCT and requires importing an XML file generated by the N1 Migration Tool. The XML files generated by the N1 Migration Tool have an .imp extension. The files for points are separate from the file for the user view. The .imp file is imported by the Metasys system Import Wizard in the SCT’s UI. The Import Wizard reads the file and creates a new Metasys system point for every point definition found in the file. The newly created points are created in the active archive database on the SCT.