The N1 Migration uses existing Metasys system Wizards to generate the N1 Mapped database. The three modes of N1 Migration are as follows:
-
online with the NIE using Auto Discovery
-
online with the NIE using the Import Wizard
-
offline with the SCT using the Import Wizard
When generating the database from the NIE, the Object Creation Wizards (Insert-Integration, Insert-Field Device, and Insert-Field Point) are used in conjunction with Auto Discovery or the Import Wizard. When generating the database from the SCT, the Import Wizard creates the N1 mapped points directly into the NIE’s archive database.