Global File - Metasys - LIT-1201535 - Supervisory Device - Network Engine

N1 Migration with the NIE Technical Bulletin

Brand
Metasys
Product name
Network Engine
Document type
Technical Bulletin
Document number
LIT-1201535
Revision date
2019-04-09
Language
English

All NCMs and OWSs on a Metasys N1 Network share the global file. The global file includes data such as system names, access or report groups, and N1 nodes. The global file contains all the data necessary to generate the system map relationship defined in the PC Groups. Only one global file exists for each network defined in an OWS; therefore, when migrating an N1 Network to an NIE, only one global file may be imported per network.

If you are importing NCMs to multiple NIEs and want them to appear in a single user view, manually edit the references for all the NCMs that are not under the Site Director.