Data Definition Language (DDL) - Metasys - LIT-1201535 - Supervisory Device - Network Engine

N1 Migration with the NIE Technical Bulletin

Brand
Metasys
Product name
Network Engine
Document type
Technical Bulletin
Document number
LIT-1201535
Revision date
2019-04-09
Language
English

DDL, a configuration language, defines the N1 Network and generates NCM databases. The N1 Migration Tool uses the global and Network Control (NC) DDL files to generate the files imported into the N1 Migration object.

Important: NIEs must reside at a higher node address on the N1 network than all NCMs and OWSs.