An archive database is the offline copy of a database, usually preserved to allow recovery from a catastrophic failure of a network device or to allow database modification without disturbing a working system.
In a Metasys N1 Network, archive databases are stored at the OWS. In a Metasys system network, archive databases are SQL databases stored on the SCT Configuration Server.