Metasys System Help - Metasys - LIT-1201535 - Supervisory Device - Network Engine

N1 Migration with the NIE Technical Bulletin

Brand
Metasys
Product name
Network Engine
Document type
Technical Bulletin
Document number
LIT-1201535
Revision date
2019-04-09
Language
English

The Metasys Help files provide shared system information and individualized mode-dependent information for the Metasys Site Management Portal (SMP) or the System Configuration Tool (SCT). The Metasys® SMP Help (LIT-1201793) provides information about alarming, commanding, auditing live data values, and other online features. The Metasys® SCT Help (LIT-12011964) provides information about offline operations such as managing archives, creating spaces, simulating systems, and establishing equipment and serving relationships.

In either SMP or SCT mode, the Metasys Help menu provides Help files in PDF format. Refer to the Johnson Controls Knowledge Exchange for the most up-to-date version of the Metasys Help files.