The NIE, defined in the N1 Network as a PC device, should now be defined as a report destination. Refer to the Defining Report/Access Groups chapter of the Operator Workstation User’s Manual (LIT-120165) for instructions on defining report destinations. Select the Destination Type PC file and enter user_app as the Destination File Name.