Note: Objects from the Metasys N1 Network with Totalizations attached to them when they were imported to the Metasys system have Totalization extensions corresponding to those Totalizations. Only the attributes described in Table 1 are migrated. Any other attribute in the NCM used as the source for Trends or Totalizations is not migrated to an NIE Trend or Totalization extension.
-
Click New in the Totalization row of the Extensions Wizard. The Insert Totalization Wizard Select Attribute screen appears.
Figure 1. Insert Totalization Wizard - Select Attribute -
Select Event Totalization or Runtime Totalization.
- Click other to display a list of attribute options.
-
Select an object in the top half of the screen and an attribute in the bottom half and click Next.
Figure 2. Insert Totalization Wizard - Select Attribute Screen -
Follow the prompts in the wizard to complete the addition of a Totalization Extension.
|
NCM Attribute |
NIE Attribute |
|---|---|
|
VALUE |
PRESENT_VALUE |
|
STATUS |
STATUS |
|
OFFLINE |
OFFLINE |
|
TROUBLE |
TROUBLE |
|
OVERRIDE |
OVERRIDDEN |