Creating a User View - Metasys - LIT-1201535 - Supervisory Device - N1 Network Engine

N1 Migration with the NIE Technical Bulletin

Product
Document number
LIT-1201535
Revision date
2019-04-09

About this task

Generate the point import files prior to creating the user view. See Creating the Import File Using the N1 Migration Tool.

Procedure

  1. Select Export User View only.
  2. Enter a name for the user view.
  3. Click the Generate Export Data button.

    The NIE and N1 Migration Object Names Screen appears. See Figure 1. This screen enables the user to assign NCMs to the NIEs before mapping the NCMs to those NIEs.

    Figure 1. NIE and N1 Migration Object Names Screen

  4. Highlight an NCM and click Edit. Enter the name of the NCM to which the NIE is mapped. The Edit NIE Name screen appears. See Figure 2.
    Figure 2. Edit NIE Name Screen

  5. Enter the name of the NIE. Click OK.

    The NIE and N1 Migration Object Names screen reappears with updated information. See Figure 3.

    Figure 3. Enter NIE and N1 Migration Object Names

  6. Click OK.
  7. The DDL Conversion Utility for N1 Migration screen appears. See Figure 4.
    Figure 4. DDL Conversion Utility for N1 Migration Screen

  8. Click OK.

    Repeat this process for each NCM and NIE to be migrated.