Trend - Metasys - LIT-1201535 - Supervisory Device - N1 Network Engine

N1 Migration with the NIE Technical Bulletin

Product
Document type
Technical Bulletin
Document number
LIT-1201535
Revision date
2019-04-09

Table 1 shows the configuration of a Trend extension. The trend is not deleted in the NCM and continues to run. If the trend is modified in either the Metasys N1 Network system or the Metasys system, the changes are not reflected in the other system. The migration occurs only at the Metasys system object addition. The Trend enable or disable default is determined by the Metasys N1 Network system default.

Table 1. Trend Migration

Metasys System Trend Object Configuration Attribute Name/Type

Metasys N1 Network Trend Configuration Variable/Type

Notes

Buffer_Size/Unsigned16

nc_samples/Unsigned 8

Number of samples both 1 – 5000

Log_Interval/Unsigned32

sample_int/Unsigned 16

NCM times are in minutes; Network Control Engine (NCE) values are in seconds.

Input_Reference/Structure

ATT_NUMBER

Convert to reference (match as best you can the attribute number).