Table 1, Table 2, Table 3, and Table 4 describe Totalization Migration. The totalization is not deleted in the NCM and continues to run. If the totalization is modified in either the Metasys N1 Network system or Metasys system system, the changes are not reflected in the other system. The migration occurs only on Metasys system object addition.
Table 1 depicts the migration of an Analog Totalization. Table 2 depicts the migration of an Event Totalization. Table 3 depicts the migration of a Pulse Totalization, and Table 4 depicts the migration of a Runtime Totalization.
|
Metasys System Analog Totalization Object Configuration Attribute Name/Type |
Metasys N1 Network Analog Totalization Configuration Variable/Type |
Notes |
|---|---|---|
|
Input_Reference/Structure |
\system\object\attr_name/char[ ] |
Convert to reference (match as best you can the attribute number). |
|
Rollover Limit/Double |
limit/Float |
|
|
Units/Enumeration |
display_units/char[7] |
Match the Metasys N1 Network unit as best you can. |
|
Low_Cutoff_Value/Float |
low_cutoff/Float |
|
|
TimeBase/Enumeration |
time_scale/Float |
|
|
ScaleFactor/Float |
display_scale/Float |
|
|
RollOver/Boolean |
TRUE |
|
|
Present Value |
Read current Totalization value from Metasys N1 Network and set. |
|
|
Add Analog Alarm object |
Report type |
Is Crit1-4 or status |
|
FAULT_ACK_REQUIRED_ATTR |
Report type |
If Crit1, 2, 3, or 4, set Metasys system attribute to True in analog alarm object. |
|
Alarm Message text |
ALARM_MSG_# |
Read Metasys N1 Network text from the number and save in alarm object. |
|
Metasys System Event Totalization Object Configuration Attribute Name/Type |
Metasys N1 Network Event Totalization Configuration Variable/Type |
Notes |
|---|---|---|
|
Input_Reference/Structure |
\system\object\attr_name/char[ ] |
Convert to reference (match as best you can the attribute number). |
|
Rollover Limit/Double |
limit/Float |
|
|
Units/Enumeration |
display_units/char[7] |
Match the Metasys N1 Network unit as best you can. |
|
Reference/Enum |
total_state/int |
|
|
Value_Per_Pulse/Float |
1 |
|
|
Scale_Factor/Float |
1 |
|
|
Transitions/Enumeration |
0 |
|
|
RollOver/Boolean |
TRUE |
|
|
Present Value |
Read current Totalization value from Metasys N1 Network and set. |
|
|
Add Analog Alarm object |
Report type |
Is Crit1-4 or status |
|
FAULT_ACK_REQUIRED_ATTR |
Report type |
If Crit1, 2, 3, or 4, set Metasys system attribute to True in analog alarm object. |
|
Alarm Message text |
ALARM_MSG_# |
Read Metasys N1 Network text from the number and save in alarm object. |
|
Metasys System Event Totalization Object Configuration AttributeName/Type |
Metasys N1 Network Pulse Totalization ConfigurationVariable/Type |
Notes |
|---|---|---|
|
Executing/Enumeration |
started/BYTE |
|
|
Input_Reference/Structure |
\system\object\attr_name/char[ ] |
Convert to reference (match as best you can the attribute number). |
|
Totalize Limit/Double |
limit/Float |
|
|
Units/Enumeration |
display_units/char[7] |
Match the Metasys N1 Network unit as best you can. |
|
Reference/Enum |
total_state/int |
|
|
Value_Per_Pulse/Float |
pulse_constant/Float |
|
|
Scale_Factor/Float |
display_scale/Float |
|
|
Transitions/Enumeration |
1 |
|
|
RollOver/Boolean |
TRUE |
|
|
Present Value |
Read current Totalization value from Metasys N1 Network and set. |
|
|
Add Analog Alarm object |
Report type |
Is Crit1-4 or status |
|
FAULT_ACK_REQUIRED_ATTR |
Report type |
If Crit1, 2, 3, or 4, set Metasys system attribute to True in analog alarm object. |
|
Alarm Message text |
ALARM_MSG_# |
Read Metasys N1 Network text from the number and save in alarm object. |
|
Metasys System Event Totalization Object Configuration Attribute Name/Type |
Metasys N1 Network Runtime Totalization Configuration Variable/Type |
Notes |
|---|---|---|
|
Input_Reference/Structure |
\system\object\attr_name/char[ ] |
Convert to reference (match as best you can the attribute number). |
|
Rollover Limit/Double |
limit/Float |
|
|
Units/Enumeration |
boolean_units/char[7] |
Match the Metasys N1 Network unit as best you can. |
|
Reference/Enum |
total_state/int |
|
|
Scale_Factor/Float |
1 |
|
|
RollOver/Boolean |
TRUE |
|
|
Present Value |
Read current Totalization value from Metasys N1 Network and set. |
|
|
Add Analog Alarm object |
Report type |
Is Crit1-4 or status |
|
FAULT_ACK_REQUIRED_ATTR |
Report type |
If Crit1, 2, 3, or 4, set Metasys system attribute to True in analog alarm object. |
|
Alarm Message text |
ALARM_MSG_# |
Read Metasys N1 Network text from the number and save in alarm object. |