Alarm Configuration Binaries/Multistates - Metasys - LIT-1201535 - Supervisory Device - Network Engine

N1 Migration with the NIE Technical Bulletin

Brand
Metasys
Product name
Network Engine
Document type
Technical Bulletin
Document number
LIT-1201535
Revision date
2019-04-09
Language
English

When migrating a Binary/Multistate object configuration, the alarm configuration attributes are read from the Metasys N1 Network system, and a Metasys system multistate alarm extension object is created as described in Table 1.

Table 1. Alarm Configuration for Binary and Multistate Objects

Metasys System Object Configuration Attribute Name/Type

Metasys N1 Network Attribute Variable/Type

Notes

NORMAL_STATE_ATTR

NOR_COND_ATTR

 

REPORT_DELAY_ATTR

DELAY_ATTR

 

NORM_ACK_REQUIRED_ATTR

NOR_RPT_ATTR

If Crit1, 2, 3, or 4, set Metasys system attribute to True.

OFFNORM_ACK_REQUIRED

_ATTR

WARN_RPT_ATTR

If Crit1, 2, 3, or 4, set Metasys system attribute to True.

FAULT_ACK_REQUIRED_ATTR

ALR_RPT_ATTR

If Crit1, 2, 3, or 4, set Metasys system attribute to True.

ALARM_MESSAGE_TEXT_ATTR

ALR_MSG_ATTR

Read Metasys N1 Network text from the number.

NUMBER_OF_STATES_ATTR

STATES_ATTR

Number of states set to 2 for Metasys N1 Network binaries.