Control logic configuration - Metasys - LIT-12012005 - Field Device - N2 Controller - 13.0

Modernization Guide for N2 Controllers - Metasys

Brand
Metasys
Product name
N2 Controller
Document type
User Guide
Document number
LIT-12012005
Version
13.0
Revision date
2023-10-16
Language
English
Table 1. Control logic comparisons
Attribute

VAV1xx

VMA1832, CVM03050

Implication

Programming Tool

HVACPro

CCT

Recreate the VAV's control logic with CCT.

Control Logic

Q/A Session for VAV Single Duct

System Selection Wizard for VAV Single Duct

Recreating the VAV's control logic should be straightforward by using the CCT System Selection Wizard or Sideloop Wizard.

Sideloop Session

Sideloop Wizard

Downloading

Locally through the Zone Bus or N2 Bus using AS-CVPRO or MM-CVT or remotely using NAE Passthrough

Locally through SA Bus using the MAP.

Must be onsite to download application using CCT.