Zone Terminal Unit considerations - Metasys - LIT-12012005 - Field Device - N2 Controller - 13.0

Modernization Guide for N2 Controllers - Metasys

Brand
Metasys
Product name
N2 Controller
Document type
User Guide
Document number
LIT-12012005
Version
13.0
Revision date
2023-10-16
Language
English

The VAV1xx controller supported an optional ZTU Zone Terminal Unit, which is not compatible and cannot be used with CVM or FEC family controllers. You can partially duplicate the Zone Terminal Unit functionality by replacing it with a DLK0350 or a DIS1710 Local Controller Display. However, the DIS1710 does not provided access to real-time clock functions such as scheduling, trending, and alarming. The DLK0350 provides access to local trends and alarms, but does not currently support schedules.