| Attribute |
UNT |
FEC |
CGM |
Implication |
|---|---|---|---|---|
|
I/O Wiring |
||||
|
Connection Location |
See Figure 1. |
See Figure 1. |
Refer to CGM General Purpose Application Controller Installation Instructions (Part No. 24-10143-01698) for information about the CGM09090 and CGM04060 controller wiring |
You can reuse the existing I/O wiring if the existing wiring is long enough to reach the controller's I/O wiring connection points. If not, you need to lengthen the wiring. |
|
Connection Type |
Spade lug connectors |
Fixed screw terminal connectors |
Pluggable screw terminal connectors |
Remove spade lug connectors from I/O wiring. |
|
N2 Wiring |
||||
|
Connection Location |
See Figure 1. |
See Figure 1. |
Refer to CGM General Purpose Application Controller Installation Instructions (Part No. 24-10143-01698) for information about the CGM09090 and CGM04060 controller wiring |
You can reuse the existing N2 wiring if the existing wiring is long enough to reach the controller's N2 connection point. If not, you need to lengthen the wiring. |
|
Connection Type |
Removable, 3-wire screw terminal connector |
Fixed screw terminal connectors |
Pluggable screw terminal connectors |
Replace the UNT's N2 wiring connector. |
|
Power Supply Wiring |
||||
|
Connection Location |
See Figure 1. |
See Figure 1. |
Refer to CGM General Purpose Application Controller Installation Instructions (Part No. 24-10143-01698) for information about the CGM09090 and CGM04060 controller wiring and see Figure 1. |
You can reuse the existing power supply wiring if the existing wiring is long enough to reach the controller's power supply connection point. If not, you need to lengthen the wiring. |
|
Connection Type |
Spade lug with removable 2-wire screw terminal connector |
Removable, 3-wire screw terminal connector |
Removable, 2-wire screw terminal connector |
Remove existing connectors from power. |
Figure 1. Wiring layout comparison of UNT versus
FEC

Note: Refer to
M4-CG Series General Purpose Application
Controller Installation Guide (Part No. 24-10143-01698) for
information about the CGM controller wiring and input and
output locations.