The external terminals on the base of DX-9100 makes it about 2 inches taller but about one inch narrower than the FAC3613. Replacement in the same enclosure space may be possible when not using all of the I/Os on the DX. Special consideration is required for DX-9100 Series controllers that mount on the face of an enclosure. You may need to find a retrofit solution such as using a new panel enclosure.
|
Dimension |
DX-9100x |
FAC3613 |
|---|---|---|
|
Height |
200 mm (7.9 in.) |
150 mm (5.9 in.) |
|
Width |
184 mm (7.2 in.) |
220 mm (8.7 in.) |
|
Depth |
100 mm (3.9 in.) |
57.5 mm (2.3 in.) |
| Value |
|---|
| N2 Compatible: enables field-conversion to N2 from MS/TP with the use of the Controller Configuration Tool (CCT). The controller can then be converted back to MS/TP at a future date. |
Consider that the onboard I/O count for an FAC3613 is slightly less than a DX-9100. As a result, you may need to add an M4-XPM or IOM Expansion I/O Module even if the old installation did not use XT/XP extension modules.
Installations that used one or more extension module sets may need extensive rearranging to accommodate the equivalent point count M4-XPMs or IOMs. Some space is regained as the XT communication module is removed.
|
Dimension |
XT Plus 1 XPs |
XT Plus 4 XPs |
IOM3711 |
|---|---|---|---|
|
Height |
118 mm (4.65 in.) |
118 mm (4.65 in.) |
150 mm (5.9 in.) |
|
Width 1 |
140 mm (5.5 in.) |
350 mm (13.8 in.) |
90 mm (3.5 in.) |
|
Depth |
57 mm (2.25 in.) |
57 mm (22.5 in.) |
53 mm (2.1 in.) |