Input and output wiring terminations of DCM FMs land on the Terminal Board (TB) assemblies on the left or right edges of the backplane.
If you reuse the enclosure, install terminal strips where you removed TB assemblies to align with existing wiring. You need to use additional wires with varying length and route them to the appropriate I/O terminals on the replacement devices.
Line power and N2 Network connections connect to the top of the backplane assembly.
Figure 1. DCM Wiring Layout