| Attribute |
AHU |
FAC3613 |
CGM09090 |
Implication |
|---|---|---|---|---|
|
I/O Wiring |
||||
|
Connection Location |
See Figure 1 . |
See Figure 1 . |
Refer to M4-CG Series General Purpose Application Controller Installation Guide (Part No. 24-10143-01698) for information about the CGM controller wiring. |
You can reuse the existing I/O wiring if the existing wiring is long enough to reach the controller's I/O wiring connection points. If not, you need to lengthen the wiring. |
|
Connection Type |
Fixed screw terminal connectors |
Fixed screw terminal connectors |
Removable screw terminal connectors |
Remove spade lug connectors from I/O wiring. |
|
N2 Wiring |
||||
|
Connection Location |
See Figure 1 . |
See Figure 1 . |
Refer to M4-CG Series General Purpose Application Controller Installation Guide (Part No. 24-10143-01698) for information about the CGM controller wiring. |
You can reuse the existing N2 wiring if the existing wiring is long enough to reach the controller's N2 connection point. If not, you need to lengthen the wiring. |
|
Connection Type |
Removable, 3-wire screw terminal connector |
Removable, 4-wire screw terminal connector |
Removable, 4-wire screw terminal connector |
Replace the AHU's N2 wiring connector with the controller's. |
|
Power Supply Wiring |
||||
|
Connection Location |
See Figure 1 . |
See Figure 1 . |
Refer to M4-CG Series General Purpose Application Controller Installation Guide (Part No. 24-10143-01698) for information about the CGM controller wiring. |
You can reuse the existing power supply wiring if the existing wiring is long enough to reach the controller's power supply connection point. If not, you need to lengthen the wiring. |
|
Connection Type |
Removable 3-wire Molex connector |
Removable, 3-wire screw terminal connector |
Removable, 2-wire screw terminal connector |
Remove existing connectors from power supply wiring and use controller's screw connector. |
Figure 1. Wiring Layout Comparison of AHU versus FAC

Note: Refer to
M4-CG Series General Purpose Application
Controller Installation Guide (Part No. 24-10143-01698) for
information about the CGM09090 controller wiring and input and output
locations.