Mounting - Metasys - LIT-12012005 - Field Device - N2 Controller - 13.0

Modernization Guide for N2 Controllers - Metasys

Product
Network and Communications > N2 Controls > N2 Controller
Document type
User Guide
Document number
LIT-12012005
Version
13.0
Revision date
2023-10-16

CGM, CVM, and FEC family controllers are not physically identical to legacy N2 controllers and have a different mounting footprint. As a result, when you use these controllers to replace legacy N2 controllers, ensure that the intended mounting location, for example, if reusing the existing control panel, it has enough space to accommodate the replacement controller. See Specific device differences and considerations for specific dimensions for legacy N2 controllers and their suggested N2-capable equipment controller replacements.

Note: Depending on the I/O count used on the legacy N2 controller, two or more physical controllers, for example, an FEC/IOM combination may be needed to replace a single N2 controller.