I/O wiring - Metasys - LIT-12012005 - Field Device - N2 Controller - 13.0

Modernization Guide for N2 Controllers - Metasys

Brand
Metasys
Product name
N2 Controller
Document type
User Guide
Document number
LIT-12012005
Version
13.0
Revision date
2023-10-16
Language
English

Several differences exist between the I/O wiring connections of the N2-capable equipment controllers and the legacy N2 controllers. Most N2-capable equipment controllers have terminals that use screw type I/O wiring connections, except for VMA models, which have spade terminals. Most legacy N2 controllers use spade lug type I/O wiring connections. You may need to modify the ends of the existing I/O wiring accordingly.

Also, N2-capable equipment controller wiring terminal locations may not line up with the existing wiring. To align wires to the corresponding N2-capable equipment controller, you may need to:

  • reroute wire from the enclosure terminal block to the N2-capable equipment controller
  • add longer wires to many of the controller terminals
  • splice additional length onto existing wire if your installation does not have a terminal block

When modifying the I/O wiring to accommodate the replacement N2-capable equipment controller, follow these recommendations, whenever possible:

  • use the same color insulation to preserve wiring standards
  • use wire of the same material and gauge
  • never splice copper to aluminum conductors without using an appropriate aluminum to copper conductor
  • use positive mechanical connections in all splices
  • follow splice manufacturer's instructions and crimp tool recommendations carefully
  • completely insulate each individual splice to protect from electrical shorts and corrosion consider using soldered connections if the enclosure location allows
  • use shrink-sleeve tubing, which provides a more reliable insulation than adhesive tape in most applications