I/O interfaces - Metasys - LIT-12012005 - Field Device - N2 Controller - 13.0

Modernization Guide for N2 Controllers - Metasys

Product
Network and Communications > N2 Controls > N2 Controller
Document number
LIT-12012005
Version
13.0
Revision date
2023-10-16

N2-capable equipment controllers have different numbers and types of onboard I/O than legacy N2 controllers. Which replacement N2-capable equipment controller you select depends on how the legacy N2 controller was applied in the field and how many I/Os were actually used by the legacy N2 controller. For more information, see Specific device differences and considerations to understand the onboard I/O differences between legacy N2 controllers and N2-capable equipment controllers.

N2-capable equipment controllers feature flexible input interfaces, allowing these controllers to support most of the same sensors supported. However, some room sensors (for example, TE-6100-11/12, TE-67xx, or TE-67xx) that are used with legacy N2 controllers feature modular (phone) jack connections. These sensors require adaptation for use with the N2-capable equipment controllers. See Specific device differences and considerations.