Downloading and commissioning - Metasys - LIT-12012005 - Field Device - N2 Controller - 13.0

Modernization Guide for N2 Controllers - Metasys

Brand
Metasys
Product name
N2 Controller
Document type
User Guide
Document number
LIT-12012005
Version
13.0
Revision date
2023-10-16
Language
English

Legacy N2 controllers support local application downloading and commissioning using the appropriate programming and commissioning tool hosted on a computer (for example, HVACPro or GX Tool), the computer's serial interface, and an RS-232 to RS-485 adapter (for example, the MM-CVT or IU-9100 or Zone Bus adapter).

N2-capable equipment controllers also support local downloading and commissioning; however, they require a different technology. For local downloading and commissioning, N2-capable equipment controllers require that CCT is hosted on a computer with a Bluetooth® interface or a third-party Bluetooth interface, and that a CWCVT or a MAP is connected to the SA Bus of N2-capable equipment controllers to toggle their protocol to N2.