Device addressing - Metasys - LIT-12012005 - Field Device - N2 Controller - 13.0

Modernization Guide for N2 Controllers - Metasys

Product
Network and Communications > N2 Controls > N2 Controller
Document number
LIT-12012005
Version
13.0
Revision date
2023-10-16

N2-configured equipment controllers support the full range of possible N2 device addresses supported by the N2 protocol standard (1 to 253); however, BACnet-configured equipment controllers only support addresses 4-127. When switching the equipment controllers from N2 to BACnet MS/TP, you may need to change your network's device addressing scheme to accommodate this limitation.