Web-based advanced reporting - Metasys - LIT-12011326 - MS-MVE-6 - MS-MVE-SC3 - MS-MVE-SCS - MS-MVE-0 - Software Application - Metasys for Validated Environments - 13.0.50

Metasys for Validated Environments on Site Management Portal Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys for Validated Environments
Document type
Product Bulletin
Document number
LIT-12011326
Version
13.0.50
Revision date
2024-11-23
Product status
Active

The Metasys Advanced Reporting System is the primary reporting tool for MVE users. You can launch the Metasys Advanced Reporting System from the ADX SMP user interface or independently from the browser. It displays the same navigation tree and user views as the Metasys Site Management Portal user interface, so no extra setup or configuration is required.

The Metasys Advanced Reporting System offers these pre-configured reports:

  • Alarm Definition

  • Trend Log Definition

  • Event Summary/Event Details

  • Controller Offline Summary/Controller Offline Details

  • Event and Audit Details

  • Trend Summary with Mean Kinetic Temperature

To generate a report, you select a report type, select which items or User View that you want to base your report on, then select the filtering criteria such as a date range. You can also create special User Views intended specifically for reporting purposes. The flexibility of the reporting system ensures that you can find the data you need.

For example, the Event and Audit Details Report is of special interest to the operator. This report displays a list of system events interlaced with user actions, enabling an auditor to determine the sequence of actions that might have led to a specific event. The list includes annotations and signatures associated with each operator action or system event, where required. This and the other reports are suitable for inspection, review, and copying by the FDA or other regulatory bodies.