Validated devices example - Metasys - LIT-12011326 - MS-MVE-6 - MS-MVE-SC3 - MS-MVE-SCS - MS-MVE-0 - Software Application - Metasys for Validated Environments - 13.0.50

Metasys for Validated Environments on Site Management Portal Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys for Validated Environments
Document number
LIT-12011326
Version
13.0.50
Revision date
2024-11-23
Product status
Active

The ADX communicates to the network engines over the IP network.

The ADX with MVE can also use a split ADX system, in which some system operations are performed on a database server and others on a web/application server computer. For more information, see the split ADX example in Metasys network and refer to the Application and Data Server (ADS/ADX) Product Bulletin (LIT-1201525).