Secure data protection - Metasys - LIT-12011326 - MS-MVE-0 - MS-MVE-6 - MS-MVE-SC3 - MS-MVE-SCS - Software Application - Metasys for Validated Environments - 13.0.50

Metasys for Validated Environments on Site Management Portal Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys for Validated Environments
Document type
Product Bulletin
Document number
LIT-12011326
Version
13.0.50
Revision date
2024-11-23
Product status
Active

Network Engines have the built-in capacity to store data locally if communication to the ADX is lost. Data critical to your facility is preserved and then archived to the database server once communication is restored. You cannot log on to an MVE validated engine to remove or clear alarms and audits.