Metasys network - Metasys - LIT-12011326 - MS-MVE-6 - MS-MVE-SC3 - MS-MVE-SCS - MS-MVE-0 - Software Application - Metasys for Validated Environments - 13.0.50

Metasys for Validated Environments on Site Management Portal Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys for Validated Environments
Document number
LIT-12011326
Version
13.0.50
Revision date
2024-11-23
Product status
Active
Figure 1. Metasys network with ADX and multiple validated engines
Figure 2. Metasys network with split ADX and multiple validated engines
Note: Non-validated engines may also be on the MVE network. However, validated systems do not support LonWorks® networks.
Note: At Release 12.0.50 and Release 13.0.50, validated engines are supported with CCM09090-0 controllers and IP devices, including the CGE series, CVE series, and FAC4911-0 equipment controllers, excluding devices with integral or remote displays.