Metasys for Validated Environments - Metasys - LIT-12011326 - MS-MVE-6 - MS-MVE-SC3 - MS-MVE-SCS - MS-MVE-0 - Software Application - Metasys for Validated Environments - 13.0.50

Metasys for Validated Environments on Site Management Portal Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys for Validated Environments
Document number
LIT-12011326
Version
13.0.50
Revision date
2024-11-23
Product status
Active

Metasys for Validated Environments (MVE) is an offering from Johnson Controls for facilities that require regulatory compliance for their environmental systems. MVE brings the flexibility and convenience of a web interface to your regulated facility. You can order the MVE application separately from the Metasys Extended Application and Data Server (ADX).

MVE is essential to facilities in which regulatory management is key to successful production. The system controls environmental conditions and audits user management for critical environments, such as clean rooms, research facilities, food production centers, and other production environments where tight control is key to product success. Whether your focus is meeting regulatory demands or reducing business risk, MVE is designed to deliver.

Figure 1. MVE electronic signature and required annotation window

Some of the many important MVE capabilities include flexible system navigation, powerful user graphics, comprehensive alarm management, trend analysis, and advanced reporting.

In addition, complex passwords and message encryption secure the system from unauthorized access and data tampering. The system adheres to Internet protocols and IT standards and is compatible with enterprise-level communication networks.

MVE is specifically designed to help customers address United States Food and Drug Administration (FDA) Title 21, Code of Federal Regulation (CFR) Part 11 compliance. MVE is also compliant with similar agencies around the world that deal with electronic records and electronic signature requirements, such as Annex 11 of the European Union Good Manufacturing Practice (EU GMP) regulations (European Medicines Agency [EMEA] 2021).

MVE software is installed on Metasys ADX, which provides the ability to configure supervisory engines as validated devices. Purchase and license MVE software separately from the ADX.

At Release 12.0.50 and Release 13.0.50, MVE is supported on Metasys UI as well as Site Management Portal (SMP).