Summary of changes - Metasys - LIT-12012115 - Server - Metasys UI - 11.0

Metasys UI Technical Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active
The following information is new or revised:
  • Updated Licensing Metasys UI features.
  • Updated the Features of the Metasys UI and Features of the Metasys UI Offline sections for the new features at Metasys Release 11.0. New Metasys UI Online features include Fault Detection and Fault Triage; Add, Delete, and Configure Objects; Show Involvement; Send Announcement; System Activity; Notification of new software availability; save and reuse Trend Studies; live trending; and Active Directory Federation Services (ADFS) integration with two-factor authentication. Show Involvement is the only new feature in Metasys UI Offline.
  • Removed references to Remote Authentication Dial-In User Service (RADIUS), because this is no longer supported at Release 11.0.
  • Updated the Troubleshooting section.
  • Updated the Metasys UI and Metasys UI Offline technical specifications.