Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active
About this task
Add annotation text to alarm events in the Metasys UI. The following procedure is an alternative
method.
Procedure
In SMP, go to Tools > Configure Preferences.
Select the Annotation Settings tab.
Click in the Annotation Text field and enter a new annotation to be added to
the list of predefined annotations. The text can be from 1 to 255 characters in
length. Click Add.
Predefined annotations can be edited or deleted. To edit or delete a
predefined annotation, click the annotation in the Predefined Annotation List.