|
Metasys UI component |
Metasys system preference setting |
|---|---|
|
Status Colors, State Colors, and Flash Settings |
Graphic Settings tab |
|
New Alarm Indicator Alarms (phone), Alarm Monitor, and Alarm Manager |
|
|
Alarm Icon based on Alarm Priority Equipment Activity widget, Alarm Panel, Alarm Monitor, and Alarm Manager |
Alarm Settings tab |
|
Alarm Sound Alarm Manager and Alarm Monitor |
Alarm Settings tab |
|
Audible Alarm |
Not a Metasys system preference setting. This is a setting for a user. , then right-click on the user and select |
|
Trend Chart Line Color and Line Markers Trend Widget and Custom Trend Viewer |
|
|
Annotations |
Annotations tab |
|
Building Network |
Metasys administrators automatically have access to the Building Network tree. To allow others users access to the Building Network tree, while in SMP: Click User Properties, check the User Can View the Item Navigation Tree (Default Tree) box. |
The Metasys UI uses settings from the Metasys system preferences. The following
table lists the components that use the Metasys system preferences.