Associating a standard graphic to an equipment object - Metasys - LIT-12012115 - Server - Metasys UI - 11.0

Metasys UI Technical Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active

About this task

The following steps presume that you are logged into SCT and your archive has spaces, equipment, Equipment Definitions, and standard graphics configured for the site. For more information about standard graphics, refer to the Metasys SCT Help (LIT-12011964) .

Any graphics associations performed in SCT require a download to the ADS/ADX/OAS to view the graphics in the Metasys UI. A download is not required to view the graphics in the Metasys UI Offline.

To associate a standard graphic to an Equipment object in SCT:

Procedure

  1. Select the Equipment object in the Equipment tree.
  2. If graphics are not already associated to device objects, then go to the Configuration tab of the Equipment object and click Edit.
  3. Select the Standard graphic from the All Items tree. Drag the Standard graphic to the Graphic attribute field.
    Note: You can have several graphics associated to an Equipment object.
  4. Click Save.