About this task
The following steps presume that you are logged into SCT and your archive has spaces, equipment, Equipment Definitions, and standard graphics configured for the site. For more information about standard graphics, refer to the Metasys SCT Help (LIT-12011964) .
Any graphics associations performed in SCT require a download to the ADS/ADX/OAS to view the graphics in the Metasys UI. A download is not required to view the graphics in the Metasys UI Offline.
To associate a standard graphic to an Equipment object in SCT: