Associating standard graphics - Metasys - LIT-12012115 - Server - Metasys UI - 11.0

Metasys UI Technical Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active
Note: In Metasys UI 2.1 and later, you can associate standard graphics to spaces or equipment in the Graphics Manager of the Metasys UI or Metasys UI Offline. You can also associate Metasys UI graphics to spaces, equipment, or Equipment Definitions. For more information, refer to Metasys UI Help (LIT-12011953) or Metasys UI Offline Help (LIT-12012116).