Associating a Graphics+ Graphic to a field controller - Metasys - LIT-12012115 - Server - Metasys UI - 11.0

Metasys UI Technical Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active

About this task

The following steps presume that you are logged into SCT and your archive has spaces, equipment, Equipment Definitions, and Graphics+ graphics configured for the site. For more information about Graphics+ graphics, refer to the Graphic Generation Tool Help (LIT-12011697).

Any graphics associations performed in SCT require a download to the ADS/ADX/OAS (and the engine, if changes were made to the engine) to view the graphics in the Metasys UI. A download is not required to view the graphics in the Metasys UI Offline.

To associate a Graphics+ graphic to field controller in SCT:

Procedure

  1. Select the field controller from the All Items tree.
  2. In the Configuration tab of the field controller, click Edit.
  3. Select the Graphics+ graphic from the All Items tree. Drag the Graphics+ graphic to the Graphic attribute field.
    Note: You can have several graphics associated to a field controller.
  4. Click Save.