About this task
The following steps presume that you are logged into SCT and your archive has spaces, equipment, Equipment Definitions, and Graphics+ graphics configured for the site. For more information about Graphics+ graphics, refer to the Graphic Generation Tool Help (LIT-12011697).
Any graphics associations performed in SCT require a download to the ADS/ADX/OAS (and the engine, if changes were made to the engine) to view the graphics in the Metasys UI. A download is not required to view the graphics in the Metasys UI Offline.
To associate a Graphics+ graphic to field controller in SCT: